ECAT.ENEMCY

Description

This parameter is used to enable or disable the EtherCAT emergency messaging.

Value Description
0 Disabled
1 Enabled

General Information

Type

NV Parameter

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

Variants Supported

EtherCAT drives: AKD2G-SPE

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

ECAT.ENEMCY

4300h

08h

Unsigned8

-

-

Read/Write

No